earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Device Administrator, ​License Administrator, AS-P
功能: 工程, SmartDriver
产品版本: 2024
2025/10/30

Gathering Server Information

You gather the license information from the field servers to identify the licenses that is to be reclaimed from the License Activation Server (FNO). The information is gathered in a file and downloaded.

You gather, and download, the license information from the field servers. This information is used to identify the licenses that is to be reclaimed from the License Activation Server (FNO).

显示更多
action_close

You reclaim licenses when you think that your licenses have been updated with new information, for example when you extend a subscription.

To reclaim licenses on Field Servers connected to Internet
  1. In Device Administrator, click Servers .

  2. Select Show licenses .

  3. Select the field servers with the licenses you want to reclaim.

  4. Click Reclaim .

  5. Click Reclaim licenses online .

  6. Click OK .

To gather server information
  1. In Device Administrator, click Servers .

  2. Select Show Licenses .

  3. Select the field servers.

  4. Click Reclaim .

  5. Click Gather server information .

  6. Click OK .

  7. In the Device information box, browse to a location where you want to save the information file.

  8. Click OK .

Move the downloaded device information file to a computer running Device Administrator that is connected to Internet and can access License Activation Server (FNO).

  • Field Server Licensing Overview
  • Reclaim Licenses
  • Reclaim Licenses for Licenses on Field Servers not Connected to Internet (FNO) Workflow
  • Gathering Server Information
  • Downloading License Information
  • Creating the Request Files
  • Uploading Request Files to License Activation Server (FNO)
  • Sending the Response Files to the Field Server when Activating or Reclaiming Licenses