earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Builder View
Functionalities: Engineering
Product version: 2023
2/12/2024

Canvas Binding Context Menu

Use the canvas binding context menu, when a binding on the canvas is selected, to select the binding in the Bindings view list or to select a type of visual style of the binding between canvas objects.

 
action_zoom_plus_stroke Canvas binding context menu
Figure: Canvas binding context menu

Table: Canvas Binding Context Menu

Command

Description

Select binding in list

Click to select the paths of the source and the target between the selected binding in the Bindings view list. For more information, see Bindings View .

Binding style

Point to and select a curved or orthogonal visual style of the bindings between objects. For more information, see Changing the Binding Style .

  • Bindings View
  • Changing the Binding Style
  • Builder View
  • Bindings