earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Sustainability
Product version: 2024, 7.0
2/23/2024

Meter Object – Basic Tab

Use the Meter object – Basic tab to configure the meter object settings.

 
action_zoom_plus_stroke Meter object – Basic tab
Figure: Meter object – Basic tab

Table: Meter Object – Basic Tab

Property

Description

Status

Displays the status of the monitored value. Read-only. For more information, see Meter Status and Meter Mode .

Mode

Displays the mode of the monitored value. Read-only. For more information, see Meter Status and Meter Mode .

Meter unit

Select the preferred unit. For more information, see Meter Object Unit .

Monitored variable (kWh)

Enter the physical meter you want to monitor.

Max value (kWh)

Enter the max value the physical meter can hold until it rolls over.

Interval (ms)

Enter the log interval.

Log size

Enter the log size.

  • Energy Consumption Overview
  • Meter Status and Meter Mode
  • Meter Object
  • Meter Object Unit