earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Sustainability
Версия продукта: 2024
23.02.2024

Consumption Signature – Expected Consumption Signature Curve Tab

Use the Consumption Signature – Expected Consumption Signature Curve tab to add and edit signature curves.

 
action_zoom_plus_stroke Consumption Signature – Expected consumption signature curve tab
Рисунок: Consumption Signature – Expected consumption signature curve tab

Таблица: Consumption Signature – Expected Consumption Signature Curve Tab

Component

Description

[ Add ]

 
action_zoom_plus_stroke

Click to add a signature curve.

[ Edit ]

 
action_zoom_plus_stroke

Click to open the signature coordinate dialog box. Более подробную информацию см. Properties – Signature Coordinate Dialog Box .

[ Remove ]

 
action_zoom_plus_stroke

Click to remove the selected signature curve.

  • Energy Consumption Overview
  • General Information Properties – Basic Tab
  • Properties – Signature Coordinate Dialog Box
  • Consumption Signature - Basic Tab
  • Consumption Signature – Input Consumption Tab
  • Consumption Signature – Output Consumption Tab
  • Consumption Signature – Expected Consumption Signature Curve Tab