earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Sustainability
Версия продукта: 2024, 7.0
10.12.2024

Consumption Signature – Output Consumption Tab

Use the Consumption Signature – Output consumption tab to view the consumption during a specific time period.

 
action_zoom_plus_stroke Consumption Signature – Output consumption tab
Рисунок: Consumption Signature – Output consumption tab

Таблица: Consumption Signature – Output Consumption Tab

Component

Description

Enable output consumption

Actual consumption

Displays the actual consumption, that is the calculated consumption from the consumption log.

Expected consumption

Displays the expected consumption, that is the expected consumption according to the signature curve.

Consumption difference

Displays the consumption difference if the consumption is higher or lower than the expected consumption.

Dependency value

Displays the dependency value, that is the calculated dependency value from the dependency log.

Period start

Period end

  • Energy Consumption Overview
  • General Information Properties – Basic Tab
  • Consumption Signature - Basic Tab
  • Consumption Signature – Input Consumption Tab
  • Consumption Signature – Output Consumption Tab
  • Consumption Signature – Expected Consumption Signature Curve Tab