earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Sustainability
Product version: 2024, 7.0
2/23/2024

Consumption Signature – Input Consumption Tab

Use the Consumption Signature – Input consumption tab to add logs and edit logs.

 
action_zoom_plus_stroke Consumption Signature – Input consumption tab
Figure: Consumption Signature – Input consumption tab

Table: Consumption Signature – Input Consumption Tab

Component

Description

Consumption log

Browse to the energy meter object that logs the actual energy consumption.

Consumption log calculation type

Select the consumption log calculation type.

For more information, see Consumption Log Calculation .

Dependency log

Browse to the dependency log that affects the energy consumption.

Dependency log calculation type

Select the dependency log calculation type.

For more information, see Consumption Log Calculation .

Calculation period

Select the period you want to compare and get the expected consumption for.

History period

Select the period you want to create the signature curve for.

  • Energy Consumption Overview
  • General Information Properties – Basic Tab
  • Consumption Signature - Basic Tab
  • Consumption Signature – Input Consumption Tab
  • Consumption Signature – Output Consumption Tab
  • Consumption Signature – Expected Consumption Signature Curve Tab