earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: Sustainability
产品版本: 2024, 7.0
2024/2/23

Meter Processor Properties – Input Dialog Box

Use the Meter Processor Properties – Input dialog box to add and calculate values from a meter object or a meter processor to a meter processor.

 
action_zoom_plus_stroke Meter processor properties – Input dialog box
图: Meter processor properties – Input dialog box

表格: Meter Processor Properties – Input Dialog Box

Property

Description

Meter

Select the meter object or meter processor you want to add to your meter processor.

Contribution

Select Add to add the meter object value to the meter process output.

Select Subtract to subtract the meter object value from the meter process output.

Percentage

Select the contribution in percentage.

  • Meter Processor
  • Meter Processor – Basic Tab