earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: Sustainability
产品版本: 2024, 7.0
2024/2/23

Meter Processor – Basic Tab

Use the Meter Processor – Basic tab to add meter objects and meter processors the meter processor.

 
action_zoom_plus_stroke Meter Processor – Basic tab
图: Meter Processor – Basic tab

表格: Meter Processor – Basic Tab

Component

Description

Status

Displays the status of the meter processor.

[ Add ]

 
action_zoom_plus_stroke

Click to add a meter object to the meter processor.

[ Edit ]

 
action_zoom_plus_stroke

Click to open the Meter Properties Input Dialog Box to edit meter objects or meter processors contributions the meter processor. 有关更多信息,请参阅 Meter Processor Properties – Input Dialog Box .

[ Remove ]

 
action_zoom_plus_stroke

Click to remove the selected meter object or meter processor from the meter processor.

Interval (ms)

Enter the log interval.

Log size

Enter the maximum log size for the meter processor.

  • Energy Consumption Overview
  • Consumption Signature – Expected Consumption Signature Curve Tab
  • Consumption Signature - Basic Tab
  • Consumption Signature – Output Consumption Tab
  • Consumption Signature – Input Consumption Tab
  • Meter Processor – Outputs Tab
  • Meter Processor – Basic Tab
  • Meter Object – Outputs Tab
  • Meter Object – Basic Tab