earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Sustainability
Версия продукта: 2024, 7.0
10.12.2024

Initiating a Meter Replacement

You initiate a meter replacement when you want to replace the physical meter that is monitored by the meter object.

Показать больше
action_close

When you replace a physical meter, you need to make adjustment to the meter object that monitor the physical meter.

Meter replacement must be planned to avoid data loss.

Use this workflow to replace a meter. Более подробную информацию см. Meter Replacement Workflow .

To initiate a meter replacement
  • Do one of the following:

    • In WorkStation, right-click the meter object, point to Meter management then click Initiate meter replacement .

    • In WebStation, right-click the meter object, then click Initiate meter replacement .

  • Meter Object
  • Meter Replacement
  • Meter Replacement Workflow