earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: Sustainability
产品版本: 2024, 7.0
2024/2/23

Finalizing a Meter Replacement

You finalize a meter replacement after you have replaced the physical meter that is monitored by the meter object. When you finalize a meter replacement, the meter object starts logging and collecting values from the physical meter.

Update the configuration of the monitored variable if the new physical meter is exposed using a different address or register.

显示更多
action_close

When you replace a physical meter, you need to make adjustment to the meter object that monitor the physical meter.

Meter replacement must be planned to avoid data loss.

Use this workflow to replace a meter. 有关更多信息,请参阅 Meter Replacement Workflow .

To finalize a meter replacement
  1. Do one of the following:

    • In WorkStation, right-click the meter object, point to Meter management then click Finalize meter replacement .

    • In WebStation, right-click the meter object, then click Finalize meter replacement .

  2. Specify the start value and the maximum value for the new meter in the dialog box.

  3. Click OK .

  • Meter Replacement
  • Meter Replacement Workflow
  • Initiating a Meter Replacement
  • Finalizing a Meter Replacement