earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Sustainability
Product version: 2024
2/23/2024

Confirming a Meter Object Settings

You confirm a meter setting after you have corrected an unexpected value.

Show More
action_close

The meter object can take different status and modes.

Meter Status

The meter object can be in two states, OK or an error state.

Meter Mode

The meter object can be in the following modes:

Normal

The meter object works as expected. It logs and calculates consumption.

Meter Replacement

A meter replacement is initiated.

For more information, see Meter Replacement .

Unexpected Meter Values

When an unexpected value is detected, the meter object enters the mode Action needed and the status of the meter object is set to inform the user that something unexpected happened.

A meter object in Action needed mode pauses the calculations and does not update the meter values.

You start the meter object again with the command Confirm meter setting .

For more information, see Confirming a Meter Object Settings .

The command Confirm meter settings open a dialog where you can change the maximum settings and set the start value of the connected meter. For example, if the mode Action needed was caused by an unexpected meter replacement.

To confirm a meter settings
  • Do one of the following:

    • In WorkStation, right-click the meter object, point to Meter management , then click Confirm meter settings .

    • In WebStation, right-click the meter object, then click Confirm meter settings .

  • Meter Status and Meter Mode