The meter processor object is used to process the information from one or many meter objects. Using the meter processor, you can add or subtract energy consumption from many different meter objects. A meter processor can also process information from another meter processor.
You can display a chart in WebStation that shows how much each connected meter object, or meter processor, contributes to the calculated result.
For more information, see Meter Processor Charts .
The meter processor has a built-in mechanism to avoid negative consumption.
For more information, see Meter Processor Suppressed Reduction .
There are three ways to handle data migration when you create a meter processor.
No migration
Migration from the newest meter start time
Migration from the oldest meter log start time
For more information, see Meter Object Data Migration in Meter Processor .