earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Sustainability
Product version: 7.0
12/19/2024

Meter Object Data Migration in Meter Processor

There are three ways to handle data migration when you create a meter processor.

  • No migration

  • Migration from the newest meter start time

  • Migration from the oldest meter log start time

 
action_zoom_plus_stroke Meter object data migration in meter processor
Figure: Meter object data migration in meter processor
No migration

Use this procedure if you want to create a meter processor with no migration.

For more information, see Creating a Meter Processor .

Migration from the newest meter log start time or the oldest meter log start time

Use this procedure if you want migration from the newest meter log start time or the oldest meter log start time.

For more information, see Creating a Meter Processor with Migration from the Newest Meter Log Start Time or the Oldest Meter Log Start Time .

  • Energy Consumption Overview
  • Meter Processor
  • Creating a Meter Processor
  • Creating a Meter Processor with Migration from the Newest Meter Log Start Time or the Oldest Meter Log Start Time