earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Sustainability
Product version: 2024, 7.0
12/10/2024

Consumption Signature Configuration Interface WebStation

Use the Consumption signature configuration interface to configure and edit the consumption signature.

 
action_zoom_plus_stroke Consumption signature configuration interface
Figure: Consumption signature configuration interface

Table: Consumption Signature Configuration Interface

Component

Description

 
action_zoom_plus_stroke

[ Pointer ]

Click to activate the pointer tool an inspect a specific value on the signature curve.

 
action_zoom_plus_stroke

[ Add regression line ]

Click to add a regression line that match all points in the selected range on the dependency axis.

 
action_zoom_plus_stroke

[ Add points ]

Click to add a point.

 
action_zoom_plus_stroke

[ Move points ]

Click to select and move a point.

 
action_zoom_plus_stroke

Remove points

Click to select and remove a point.

Consumption

Click to configure the axis for consumption.

Dependency

Click to configure the axis for dependency.

 
action_zoom_plus_stroke

[ Zoom to fit ]

Click adapt the signature to the area.

  • Consumption Signature
  • Consumption Log Calculation
  • Consumption Signature Configuration Interface WebStation