earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Sustainability
Product version: 2024, 7.0
2/23/2024

Consumption Signature – General Tab

Use the Consumption Signature – General tab to configure the consumption signature.

 
action_zoom_plus_stroke Consumption Signature – General tab
Figure: Consumption Signature – General tab

Table: Consumption Signature – General Tab

Component

Description

Note 1

Type text that you display in a graphic or use when searching for the object.​

Note 2

Type text that you display in a graphic or use when searching for the object.​

Consumption log

Browse to the energy meter object that logs the actual energy consumption.

Consumption log calculation type

Select the consumption log calculation type.

For more information, see Consumption Log Calculation .

Dependency log

Browse to the dependency log that affects the energy consumption.

Dependency log calculation type

Select the dependency log calculation type.

For more information, see Consumption Log Calculation .

Calculation period

Select the period you want to compare and get the expected consumption for.

Period

Select the period you want to create the signature curve for.

Enable output consumption

Enable or disable the output consumption values.

  • Consumption Signature
  • Consumption Log Calculation
  • Consumption Signature Configuration Interface WebStation