This section provides recommendations on wire sizes and lengths for the CRS-HH-REL-10 relay module.
The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.
Terminals |
Minimum Cross-sectional Area |
Maximum Cable Length |
Relay output terminals (DO1 to DO10) a |
According to local wiring rules b |
According to local wiring rules b |
Digital input terminals (DI1 to DI12) c |
0.34 mm² (22 AWG) |
200 m (650 ft) |