earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: License Administrator, License Server
Funkcje: Zarządzanie licencją
Wersja produktu: 3.2, 3.3, 2022, 2023
2024-11-29

Activating EcoStruxure Building Operation Software Licenses

You activate EcoStruxure Building Operation software licenses, from the License Activation Server, to make EcoStruxure Building Operation software licenses available.

Uwaga
  • This procedure requires that an entitlement with the licenses has been received. Więcej informacji zawiera Order Information Request .

    For more information on how to place an order, contact your EcoStruxure Building Operation vendor.

Pokaż więcej
action_close

Use this workflow to add licenses for EcoStruxure Building Operation software running on Windows.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Licensing workflow
Rysunek: Licensing workflow
EcoStruxure Building Operation Software Licensing Installation and Location

Read the setup guide for installation and location of License Server and License Administrator.

Więcej informacji zawiera EcoStruxure Building Operation Software Licensing Installation and Location .

Install License Administrator and License Server

Install Licenses Administrator and License Server.

Więcej informacji zawiera Installing the License Administrator and the License Server .

Start License Administrator

Start License Administrator.

Więcej informacji zawiera Starting License Administrator .

Activate EcoStruxure Building Operation Software Licenses

Activate EcoStruxure Building Operation Software Licenses.

Więcej informacji zawiera Activating EcoStruxure Building Operation Software Licenses .

Configure License Server Recovery Settings

Configure License Server to restart if it unexpectedly stops.

Więcej informacji zawiera Configuring the License Server Recovery Settings   .

To activate EcoStruxure Building Operation software licenses
  1. In License Administrator, click the Licenses tab.

  2. On the Licenses toolbar, click the Add license from entitlement ID button

     
    action_zoom_plus_stroke
    .

  3. In the Add License dialog box, in the Enter license entitlement ID box, type the entitlement ID that contains the licenses to activate. The entitlement ID is printed on the entitlement.

  4. Click OK .

  5. In the Licenses View, in the Activate column, select the number of license to activate.

  6. Click Activate .

  7. Click Close .

  8. Click Restart now to restart the License Server and activate the license.

The activated licenses are now available on the License Server.

  • EcoStruxure Building Operation Software Licensing Installation and Location
  • EcoStruxure Building Operation Software Licensing Workflow