earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2.0, 2.1, 3.0, 3.1
12/11/2018

Add Cause Note Dialog Box

Use the Add Cause Note dialog box to add a cause note.

 
action_zoom_plus_stroke Add Cause Note dialog box
Figure: Add Cause Note dialog box

Table: Add Cause Note Dialog Box

Component

Description

Name

Type the name of the cause note.

Group name

Enter the cause note group the cause note belongs to.

Description

Type a description of the cause note.

  • User Actions
  • Control Panel
  • Cause Notes
  • Alarm Control Panel – Cause Notes View