earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Tendências
Versão do produto: 3.2, 3.3, 2022
15-10-2020

Add Trend Log Record Dialog Box

Use the Add trend log record dialog box to add a trend log record to a trend log.

 
action_zoom_plus_stroke Add trend log record dialog box
Imagem: Add trend log record dialog box

Tabela: Add Trend Log Record Dialog Box

Component

Description

Time stamp

Enter the time and date of the new record.

Value

Enter the value of the new record.

Comment

Type a comment for the record.

  • Trend Log Types
  • Manual Trend Logs
  • Adding a Trend Log Record to a Manual Trend Log
  • Manually Adding a Trend Log Record to a Trend Log
  • Manually Adding a Trend Log Record to a Trend Log List
  • Trend Log Lists
  • Editing or Commenting a Trend Log Record
  • Edit/Comment Trend Log Record Dialog Box