earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-C, AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Server, Project Configuration Tool
功能: 时间表
产品版本: 1.8
2016/10/13

Adding a Date Calendar Event

You add a date to a calendar to specify an exception date for a specific day, such as 7 May, 2013.

显示更多
action_close

The dates specified in a calendar are shown in the date list. You can specify dates in a calendar by three different methods:

  • Date: a specific date

  • Date range: a fixed period with a set start and stop date

  • Calculated date: a fixed period that repeats

Date Calendar Events

A single date within a calendar is an entry that occurs once or every year on the same date.

The following single date entry choices schedule an event on a single date, January 1, 2009:

  • Year - 2009

  • Month - January

  • Day of month - 1

  • Day of week - Any day

The following single date entry choices schedule an event on a single date every year, January 1:

  • Year - Any Year

  • Month - January

  • Day of month - 1

  • Day of week - Any day

The following choices produce an error message:

  • A day, month, and year combination that does not coincide

    An example is Friday, March 5, 2009. This date actually falls on a Thursday.

  • Any years past 2105

  • An explicit day that is out of range

    An example is September 31 or February 29 in a non-leap year.​​

Date Range Calendar Events

You can include a date range in the date list. A date range is a series of days to include in a calendar. An example of a date range is January 1, 2009 to January 31, 2009, which adds the entire month of January to the calendar as an event. You can use this date range for a device, such as a thermostat, to behave differently for the whole month of January.

Calculated Calendar Events

You can include a calculated date on a date list. A calculated date has no set start and stop date. For example, you use a calculated date to schedule the first week of the even months on a Friday.

To add a date calendar event
  1. In WorkStation, in the System Tree pane, select the calendar you want to add the exception to.

  2. Click the Calendar Editor tab.

  3. On the Calendar Editor toolbar, click the Add Date button

     
    action_zoom_plus_stroke
    .

  4. In the Entry name box, type the name that you want to display on the date list.

     
    action_zoom_plus_stroke
  5. In the Year box, select the year for the date.

  6. In the Month box, select the month for the date.

  7. In the Day of month box, select the day for the date.

  8. In the Day of week box, select the weekday for the date.

     
    action_zoom_plus_stroke
  9. Click OK .

  10. On the File menu, click Save .

  • Adding a Date Range Calendar Event
  • Adding a Calculated Date Calendar Event
  • Creating a Calendar
  • Adding a Calendar Exception Event
  • Edit Calendar Entry Dialog Box – Add Date
  • Calendar Events
  • Calendars in WorkStation
  • General Information Properties – Basic Tab
  • References Tab