earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-B, Edge Server, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Fonctionnalités : Calendriers
Version produit : 3.2, 3.3, 2022, 2023
21/05/2024

Ajout d'un événement spécial Date

Vous ajoutez un événement spécial date simple pour créer une exception pour un jour spécifique du calendrier, par exemple le 10 décembre 2013.

Afficher plus
action_close

An exception event occurs instead of the scheduled weekly events for a single date, date range, calculated date, or calendar reference.

For example, you create an exception event in March for an intense aerobics class in the gym to open an air vent to 100 % from 06:30 to 17:00 every Wednesday in March. This exception event takes precedence over the regularly scheduled weekly Wednesday events.

When scheduling exception events, you can use four exception types to provide flexibility and control in your schedule.

Date Exception Events

A single date exception event can occur on a single day, or you can use the options for the event to occur on more than one day. The options such as Any year and Any day provide flexibility. To schedule a single date event to take place every year on October 31, you select the following single date options:

  • Year: Any year

  • Month: October

  • Day of month: 31

  • Day of week: Any day

Date Range Exception Events

A date range exception event is an event that lasts over a period of time. In addition to a specific day of month, you can select Odd, Even , or Any month , and Any day or Last day , to provide the flexibility to a date range. For example, to schedule an exception event to occur annually from the last day of March to the last day of April, select the following options for the start and end dates:

Start Date
  • Start year: Any year

  • Start month: March

  • Day of month: Last day

  • Day of week: Any day

End Date
  • Year: Any year

  • Month: April

  • Day of month: Last day

  • Day of week: Any day

Calculated Exception Events

A calculated date is an exception event that recurs. Other than a specific month and week, you can select Any month and Any week or Last week , to provide flexibility to a calculated date. For example, to schedule the Monday of the first week of every month for an exception event, select the following options:

  • Month: Any month

  • Week of month: First week

  • Day of week: Monday

Calendar Exception Events

A calendar reference allows you to apply an exception event for all dates specified in the calendar. For example, to schedule exception events for all holidays on a calendar, you select the calendar you want to reference and the schedule will follow the holidays created in the calendar.

Pour ajouter un événement spécial de date
  1. Dans WorkStation, dans le volet arborescence du système , sélectionnez le programme horaire auquel vous souhaitez ajouter l'événement d'exception de date simple.

  2. Cliquez sur l'onglet Basique .

  3. Sur la barre d'outils Éditeur d'horaire basique , cliquez sur le bouton Nouvel événement d'horaire

     
    action_zoom_plus_stroke
    .

  4. Cliquez sur Exception .

  5. Dans la boîte de dialogue Propriétés de l'événement horaire , sous Type d'exception , cliquez sur Date simple .

  6. Sélectionnez Toute la journée si l'événement d'exception doit être actif ou non pendant toute la journée.

  7. Dans la colonne Heure de début , saisissez une heure de début pour l'événement d'exception.

  8. Dans la colonne Heure de fin , saisissez une heure de fin pour l'événement d'exception.

  9. Dans la colonne Valeur , sélectionnez une valeur pour l'événement d'exception.

  10. Dans le champ Nom , saisissez un nom pour l'événement d'exception.

  11. Dans le champ Priorité , sélectionnez une priorité pour l'événement spécial pour qu'il outrepasse les événements en conflit dont les priorités sont inférieures.

  12. Dans le champ Année , sélectionnez l'année de la date simple.

  13. Dans le champ Mois , sélectionnez le mois de la date simple.

  14. Dans le champ Jour du mois , sélectionnez un jour du mois pour la date simple.

  15. Dans le champ Jour de la semaine , sélectionnez un jour de la semaine pour la date simple.

  16. Cliquez sur OK .

  17. Dans le menu Fichier , cliquez sur Enregistrer .

  • Schedule Events
  • Exception Events in WorkStation
  • Schedule Event Properties Dialog Box – Single Date Exception View