earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 2023
12/17/2022

Creating a Hyperlink

You create a hyperlink in WorkStation to get easy access to important information on the Internet.

Show More
action_close

EcoStruxure Building Operation software supports hyperlinks. Hyperlinks are added only in WorkStation. In WorkStation, you open hyperlinks in the workspace or in a web browser. In WebStation, hyperlinks always open in a new tab of the web browser. In the WorkStation workspace, you navigate through the web page in the same way you would in a web browser.

WorkStation uses the following built-in web browsers to display web pages:

  • Microsoft Internet Explorer is used in 4.0.1 and all previous versions of WorkStation.

  • Chromium Edge is used in 4.0.2 and all subsequent versions of WorkStation.

 
action_zoom_plus_stroke The EcoStruxure Building Operation software supports hyperlinks
Figure: The EcoStruxure Building Operation software supports hyperlinks

To create a hyperlink
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server or folder where you want to create the hyperlink.

  2. On the File menu, point to New object and then click Hyperlink .

  3. In the Create New Object dialog box, in the Name box, type a name for the hyperlink.

  4. In the Description box, type a description for the hyperlink.

  5. Click Edit in wizard button.

  6. In the Assign the URL page, in the URL box, type the URL for the hyperlink.

    Important:

    You have to include http:// or https:// in the URL.

  7. In the Open externally box, select True to open the hyperlink in your computer's default browser.

    Note:

    When the hyperlink is displayed in the browser, the WorkStation workspace displays Hyperlink Properties - Basic view.

  8. Click Create .

  • Hyperlinks
  • Create Object Dialog – Naming the Object Page
  • Create Hyperlink Wizard – Assign the URL Page
  • Hyperlink Properties Dialog Box – Basic Tab