earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
功能: 趋势
产品版本: 2024, 7.0
2024/12/3

Adding a Real-Time Trend Series to a Trend Chart

You add a real-time trend series to a trend chart to compare trend data from different logs or variables.

显示更多
action_close

In a trend chart, a series can be presented as a line, discrete line, digital, or bars. In a trend chart, series can be presented in different colors and with different line weights.

In WorkStation, in a multi trend log list, series are presented as text and can be exported to .XML or .CSV.

 
action_zoom_plus_stroke Types of series presentation, schematic
图: Types of series presentation, schematic

To make reading easier in a trend chart, records can be presented with markers. Markers can only be shown for lines and discrete lines, not for digital or bars.

 
action_zoom_plus_stroke Presentation with markers, schematic
图: Presentation with markers, schematic

To add a real-time trend series to a trend chart
  1. In WorkStation, in the System Tree pane, select the trend chart you want to add a trend series to. ​

  2. On the File menu, click Properties .

  3. In the Trend Chart Properties dialog box, under Series Configuration Settings , click the Add button

     
    action_zoom_plus_stroke
    .

  4. In the Create Object wizard, in the object type list, select Real Time Trend Series .

  5. In the Name box, type a name for the series.

  6. In the Description box, type a description for the series.

  7. Click Next .

  8. In the Configure Real-time Trend Series page, in the Display variable box, enter the path to the variable you want to display in the trend chart.

  9. In the Weight box, enter the line weight of the series.

  10. In the Show markers box, select True to display a marker for each recorded value.

  11. Click Create .

  12. Click OK .

  • Trend Series
  • Trend Chart Properties
  • Create Object Dialog – Naming the Object Page
  • Create Trend Chart Wizard – Configure Real-Time Trend Series Page
  • Removing a Trend Chart Series
  • Trend Chart View