earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WorkStation
功能: 趋势
产品版本: 2024, 7.0
2024/12/2

Removing a Trend Chart Series

You remove unused series from the trend chart.

显示更多
action_close

Trend charts are a way to graphically present trend logs. A trend chart can contain one or more trend logs that are represented in the trend chart by lines or bars.

You can also add and remove trend logs from a trend chart. This makes it easy to compare different trend logs, for example the energy consumption compared to the average temperature.

 
action_zoom_plus_stroke Trend chart in WorkStation
图: Trend chart in WorkStation

Trend Chart Navigation in WorkStation

The trend chart contains a lot of tools for easy navigation in the chart. You can scroll or use the predefined settings to focus on the time span you want to see.

有关更多信息,请参阅 Trend Chart Navigation in WorkStation .

Trend Chart Navigation in WebStation

The trend chart contains a lot of tools for easy navigation in the chart. You can scroll or use the predefined settings to focus on the time span you want to see.

有关更多信息,请参阅 Trend Chart Navigation in WebStation .

Trend Chart Series in WorkStation

You can display the trend logs as trend log series in a trend chart in a number of ways. For example, you can change the color and weight of the trend log line, or display markers at the time where the trend log value was sampled.

有关更多信息,请参阅 Trend Chart Series in WorkStation .

Trend Chart Series in WebStation

You can display the trend logs as trend log series in a trend chart in a number of ways. For example, you can change the color and weight of the trend log line, or display markers at the time where the trend log value was sampled.

有关更多信息,请参阅 Trend Chart Series in WebStation .

Trend Chart Axes in WebStation

​A trend chart displays the records of a trend log or an extended trend log as a series.

有关更多信息,请参阅 Trend Charts .

To remove a trend chart series
  1. In WorkStation, in the System Tree pane, select the trend chart from which you want to remove a series.

  2. On the Trend Chart , click the Series tab.

  3. In the Series area, right-click a series and select Remove series .

The selected series is now removed from the trend chart.

  • How Trend Logs Work
  • How Trend Charts Work
  • Trend Chart Event Icons
  • Opening a Trend Log List
  • Refreshing a Trend Log List
  • Changing the Color of a Trend Chart Series
  • Changing the Line Weight of a Trend Chart Series
  • Showing Markers in a Trend Log Series
  • Viewing Events in a Trend Chart
  • Hiding a Series in a Trend Chart
  • Changing the Display Order of a Trend Chart Series
  • Displaying Trend Log List Values as Decimals
  • Displaying Trend Log List Values as Bitstrings