earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 1.9
2016/12/14

Adding a User Account to a User Account Group

You add a user account to a user account group to add software permissions and workspaces to a user.

显示更多
action_close

A user account can be a member of one or more user account groups and belongs to a particular domain.

User Accounts

A user account uniquely identifies a user to the system. When setting up user accounts, keep the following points in mind:

  • Configure as few settings as possible at the user account level.

  • Assign a required user name and password, which the system uses for identification and authentication purposes. 有关更多信息,请参阅 Password Administration .

  • The user account is unique within the domain it belongs to. For example, an admin user account is located in Domain A. This account cannot be used to administrate Domain B. 有关更多信息,请参阅 Domains .

  • Manage accounts at the domain level using a default administrator account. 有关更多信息,请参阅 Administration Accounts in SmartStruxure Server Local Domain .

  • Track user activity at the user-account level. 有关更多信息,请参阅 Audit Trailing of User Activity .

User Account Groups

A User Account Group can contain both user accounts and other user account groups. To facilitate the creation and administration of users, assign software permissions and workspaces to user account groups instead of individual user accounts.

In this example, Paul is a member of the Janitor group and the Administrator group. His account inherits the software permissions and workspaces of both groups. Susan is a member of the Administrator group and inherits the software permissions and workspaces of the Administrator group.

 
action_zoom_plus_stroke A user account belongs to a domain and is a member of one or more user account groups
图: A user account belongs to a domain and is a member of one or more user account groups
注释:
  • Although user accounts are members of user account groups, they are not physically stored in user account groups. Instead, user accounts and user account groups are parallel entities so that individual accounts can be members of one or more groups.

Windows Active Directory User Groups

You can map Windows Active Directory groups to Building Operation user account groups if Building Operation runs on a network that uses this directory to manage users and user account groups. A Building Operation user account group that includes a Windows account group can be member of another Building Operation user account group.

有关更多信息,请参阅 Windows Active Directory User Groups .

WorkStation Account Management

​As a WorkStation administrator, you can change passwords, track user activities, validate accounts, and set up user and user and user group accounts.

有关更多信息,请参阅 WorkStation Account Management .

To add a user account to a user account group
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the SmartStruxure server.

     
    action_zoom_plus_stroke
  3. Click Account management .

  4. In the Domain list, select the domain the user account belongs to.

     
    action_zoom_plus_stroke
  5. In the User Accounts list, select the user account you wish to add to a user account group.

  6. Click Group membership .

  7. In the Available User Account Groups list, select a user account group and click the Add button

     
    action_zoom_plus_stroke
    .

     
    action_zoom_plus_stroke
  8. On the File menu, click Save .

  • Software Permissions and User Account Groups
  • User Account – Group Membership Tab
  • Adding a User Account to a User Account Group
  • User Accounts and User Account Groups