earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WorkStation
Funkcje: Alarmy
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-05-18

Adding an Action Note to an Alarm

You add an action note to an alarm to let others know what you have done to correct the problem that caused the alarm.

Pokaż więcej
action_close

An action note is a predefined note that contains information on what you have done to solve the problem that triggered the alarm.

You can add an action note to an alarm. In some cases, adding an action note to an alarm is optional. In other cases, you are required to enter an action note when you acknowledge the alarm.

You add an action note using WorkStation or WebStation. You can view an action note added to an alarm in WorkStation or WebStation.

To add an action note to an alarm
  1. In WorkStation, in the Alarms pane, right-click the alarm and then click Add action note .

  2. In the Action Notes dialog box, select the action note.

  3. Click OK .

The action note is added to the alarm.

  • Action Notes
  • Action Notes Dialog Box
  • Viewing an Action Note
  • Alarms Pane and Alarm View
  • Alarms Pane Context Menu
  • Alarms Pane and Alarm View Toolbar