earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Server, Virtual Project Servers
Functionalities: Alarms
Product version: 1.8
4/29/2021

Alarm Functions

arrow1_rotationAlarm Filter Conditions arrow1_rotationTime Delay arrow1_rotationShunt Variable arrow1_rotationDeadband arrow1_rotationAlarm Messages arrow1_rotationPriority arrow1_rotationCategories arrow1_rotationAcknowledgements arrow1_rotationUser Actions arrow1_rotationNotifications arrow1_rotationAutomatic Assignments arrow1_rotationUnit of Measure in Alarms arrow1_rotationAlarm Attachments

You can monitor variables and configure the alarms in many different ways. You can, for example, connect the alarm to a shunt variable, add dead band to the alarm limit, or configure the priority of the alarm.

Alarm Filter Conditions

Alarm filter conditions are used to set up the conditions for the alarms you want to be displayed in an Alarms pane or an Alarm View. You also use alarm filter conditions to determine the conditions that have to be met before a sum alarm is triggered, an email notification is sent, a write to file notification is written, or an alarm is automatically assigned to a user.

For more information, see Alarm Filter Conditions .

Time Delay

Time delay prevents unintentional activation-deactivation cycles. You can delay the time before the alarm is triggered when the alarm state goes from normal state to alarm state and when it goes from alarm state to reset state.

For more information, see Time Delay .

Shunt Variable

​A shunt variable is a binary value that works as an on/off switch for the alarm.

For more information, see Shunt Variables .

Deadband

​Deadband is an area of the alarm range where no reset action occurs. The purpose of the deadband is to prevent unintentional activation-deactivation cycles.

For more information, see Deadband .

Alarm Messages

​When configuring the alarm, you can write a message that displays in the Alarms pane, Events pane, Alarm Views, and Event Views when an alarm is triggered or reset.

For more information, see Alarm Messages .

Priority

​When configuring an alarm, you define the priority of the alarm. The priority is used to inform the operator of the importance of the triggered alarm. The priority is displayed in the Alarms pane, Events pane, Alarm Views, and Event Views.

For more information, see Priority .

Categories

​You can group together alarms in categories to simplify the identification of the alarm. When the alarm is triggered, the category name is displayed together with the alarm in the Alarms pane, Events pane, Alarm Views, and Event Views.

For more information, see Categories .

Acknowledgements

​When an alarm is triggered, you acknowledge the alarm to indicate to other users that you have responded to the alarm and intend to troubleshoot the problem that caused the alarm. The name of the user that acknowledges the alarm is displayed in the Alarms pane, Events pane, Alarm Views, and Event Views.

For more information, see Acknowledgements .

User Actions

​You can add information when handling a trigger alarm. For example, you can add a comment to the alarm or open an action note that is connected to the alarm. When configuring an alarm, you can force the user to perform different actions when handling a triggered alarm.

For more information, see User Actions .

Notifications

Notifications are used for notifying users or user groups that a certain alarm or other event, such as a schedule or an application condition, has occurred in the system. ​The notification contains a prewritten message that can be displayed as a popup message, sent as an email, sent to an SNMP manager, or written to a text file.

For more information, see Notifications .

Automatic Assignments

A triggered alarm can be automatically assigned to a specific user or user group that is most suited to correct the problem. An assigned alarm indicates to other users that someone is working with the problem that caused the alarm. The name of the user that is assigned to the alarm and the assignment status are displayed in the Alarms pane, Events pane, Alarm Views and Event Views.

For more information, see Automatic Assignments .

Unit of Measure in Alarms

When creating an alarm, the alarm limit and deadband values inherit the unit of the monitored variable. You can change the unit of the alarm to any unit within the same unit category as the monitored variable.

Note:

You cannot define a unit to an alarm that monitors a unitless variable.

For more information, see Unit of Measure in Alarms .

Alarm Attachments

You can add attachments to alarm objects, except System Information alarms. An attachment is a link pointing to an object in the system. When an alarm that has an attachment is triggered, a paperclip icon is displayed in the Alarms pane and Alarm Views. It is also possible to configure the attachment to display when the alarm is going from Normal to Alarm state.

For more information, see Alarm Attachments .

  • Alarms Overview
  • Alarm Filter Conditions
  • Shunt Variables
  • Categories
  • Priority
  • Time Delay
  • Deadband
  • Alarm Messages
  • Acknowledgements
  • User Actions
  • Notifications
  • Automatic Assignments
  • Unit of Measure in Alarms
  • Alarm Attachments
  • Create Alarm Wizard – Attachment Page
  • Alarms Pane and Alarm View Toolbar
  • Adding an Attachment to an Alarm
  • Adding an Attachment to Multiple Alarms