earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Server, Virtual Project Servers
Functionalities: Alarms
Product version: 1.8
10/13/2016

Alarms Overview

arrow1_rotationAlarm States arrow1_rotationAlarm Types arrow1_rotationAlarm Functions arrow1_rotationAlarm Objects in Multiple Servers arrow1_rotationAlarms Pane and Alarm View Customization arrow1_rotationAlarm Filter Conditions arrow1_rotationMass Create

You use an alarm to monitor a variable and to alert you if the monitored variable matches the configured alarm conditions.

You can configure an alarm to send a message to a specified user or user group when the alarm is triggered or force the user that acknowledges the alarm to write a cause note. You can also configure the alarm to flash and play a sound when it is triggered.

Suppose you want to monitor the temperature of a freezer protector on a compressor. You create an alarm that triggers when the temperature drops too low. A message is automatically sent to an assigned operator who acknowledges the alarm and corrects the problem.

 
action_zoom_plus_stroke Triggered, reset, and acknowledged alarms presented in Alarms pane
Figure: Triggered, reset, and acknowledged alarms presented in Alarms pane

Alarm States

​An alarm is always in a certain alarm state. The state of the alarm is presented in the alarm properties, in the Alarms pane, or in the Alarm Views.

For more information, see Alarm States .

Alarm Types

An alarm compares the value from a monitored variable with the conditions of the alarm. Different types of alarms handle different types of variables and different forms of evaluation.

For more information, see Alarm Types .

Alarm Functions

You can monitor variables and configure the alarms in many different ways. You can, for example, connect the alarm to a shunt variable, add dead band to the alarm limit, or configure the priority of the alarm.

For more information, see Alarm Functions .

Alarm Objects in Multiple Servers

In a multi-server system, you create alarm objects on the Enterprise Server. These objects, such as checklists and action notes, are inherited by the SmartStruxure server devices that are connected to that Enterprise Server. The copies on the connected SmartStruxure server devices are read-only, so in order to edit them you must edit their source objects on the Enterprise Server. One advantage with this is that you can display the objects and their content on the SmartStruxure server devices even if the Enterprise Server goes offline.

For more information, see Alarm Objects in Multiple Servers .

Alarms Pane and Alarm View Customization

You use the Alarms pane and the Alarm View to view and administer alarms. When an alarm is triggered, it is displayed in the Alarms pane or Alarm Views together with information about the alarm. You can edit the Alarm View filter to display the Alarm View only when certain alarms are triggered. You can create and use more than one Alarm View. The Alarms pane and each Alarm View can be customized with an alarm filter to show information that is relevant to the user who supervises the alarms. Customized settings are lost when you perform a system upgrade.

For more information, see Alarms Pane and Alarm View Customization .

Alarm Filter Conditions

Alarm filter conditions are used to set up the conditions for the alarms you want to be displayed in an Alarms pane or an Alarm View. You also use alarm filter conditions to determine the conditions that have to be met before a sum alarm is triggered, an email notification is sent, a write to file notification is written, or an alarm is automatically assigned to a user.

For more information, see Alarm Filter Conditions .

Mass Create

You use the mass create feature to create multiple identical alarms or trend logs for different objects, instead of creating the alarms or trend logs one by one. From trend logs, you can mass create extended trend logs.

For more information, see Mass Create .

  • Function Overview
  • Alarm Types
  • Alarm Objects in Multiple Servers
  • Alarm Functions
  • Alarm States
  • Alarms Pane and Alarm View Customization
  • Alarm Filter Conditions
  • Mass Create