earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Virtual Project Servers
Functionalities: Alarms
Product version: 2024, 7.0
12/3/2024

Alarms Pane and Alarm View Toolbar

Use the Alarms pane and Alarm View toolbar to manage the alarms.

Table: Alarms Pane and Alarm View Toolbar

Button

Description

 
action_zoom_plus_stroke

Acknowledge

​Click to acknowledge alarm state or reset state.

For more information, see Alarm Acknowledgements .

 
action_zoom_plus_stroke

Enable alarm

​Click to enable the alarm. If the alarm state changed, for example, from alarm state to normal state during the time the alarm was disabled, the alarm is given the new state once it is enabled.

For more information, see Disable and Enable Alarms .

 
action_zoom_plus_stroke

Disable alarm

​Click to disable the alarm. The alarm is inactivated and cannot be acknowledged or reset until it is enabled.

For more information, see Disable and Enable Alarms .

 
action_zoom_plus_stroke

Unhide alarm

​Click to show the alarm.

For more information, see Hide and Show Alarms .

 
action_zoom_plus_stroke

Hide alarm

​Click to hide the alarm in the Alarms pane or Alarm View. The alarm is still logged in the Event log.

For more information, see Hide and Show Alarms .

 
action_zoom_plus_stroke

Add comment

​Click to add a comment to the alarm.

For more information, see Alarm Comments .

 
action_zoom_plus_stroke

Add cause note

​Click to add a cause note to the alarm.

For more information, see Cause Notes .

 
action_zoom_plus_stroke

Add action note

​Click to add an action note to the alarm.

For more information, see Action Notes .

 
action_zoom_plus_stroke

Checklist

​Click to view the checklist for the alarm.

For more information, see Checklists .

 
action_zoom_plus_stroke

Show disabled alarms

​Click to toggle between showing and hiding disabled alarms.

For more information, see Disable and Enable Alarms .

 
action_zoom_plus_stroke

Show hidden alarms

​Click to toggle between hiding alarms and showing hidden alarms.

For more information, see Hide and Show Alarms .

 
action_zoom_plus_stroke

Go to alarm object

​Click to open the settings of the alarm in the Work Area.

 
action_zoom_plus_stroke

Edit user filter

Click to select the conditions for the temporary alarm display in the Alarms pane. When you close the view, the filter conditions are lost. For more information, see Alarm Filters .

 
action_zoom_plus_stroke

Favorites

Click to open the Favorites menu where you select, add, and manage favorites.

  • Alarm Acknowledgements
  • Disable and Enable Alarms
  • Hide and Show Alarms
  • Alarm Comments
  • Cause Notes
  • Action Notes
  • Checklists
  • Group and Sort Objects
  • Alarm Filters
  • Alarm and Event Details
  • Alarms Pane and Alarm View
  • Alarms Pane Context Menu
  • Alarms Pane and Alarm View Customization