The Alarms Per Server report provides information about the number and type of alarms that have been triggered for a particular EcoStruxure BMS server. You can use the report to identify the most frequent alarms on a particular EcoStruxure BMS server and then benchmark the operations of your building system. For example, suppose there are numerous alarms in Building A, but more staff are present in Building B. The report could indicate that you need to increase the staff in Building A in order to meet the operational needs of the building.
The following table shows the input parameters for the report.
Input Parameters |
Description |
Start report date/time |
Specifies the start date and time of the triggered alarms. |
End report date/time |
Specifies the end date and time of the triggered alarms. |
Date range filter |
Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent. For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days. Select Fixed date if you entered a Start report date/time and an End report date/time . |
Acknowledged only |
Specifies whether you want to report on Acknowledged alarms only or to report on all alarm activity. |
Server |
Specifies the EcoStruxure BMS server that manages the alarms. |
Report view |
Specifies the format, such as a table, for displaying the report. |
Show top |
Specifies a number used to filter the top most frequently occurring alarms. |