earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: WebReports
Funktionaliteter: Rapporter
Produktversion: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
2021-12-16

Assign Default Reports Page

Use the Assign Default Reports page to assign a template to a type of object. The template is then used when you generate a default report in WorkStation. Mer information finns i WebReports Main Page .

 
action_zoom_plus_stroke Assign Default Reports page
Figur: Assign Default Reports page

Tabell: Assign Default Reports Page

Component

Description

Type of Object

Lists the type of objects associated with the templates.

Default Report Templates

Select to assign a template to a type of object. The template is used when you generate a default report.

  • Default Reports
  • WebReports Main Page