earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 3.2, 3.3, 2022
30/04/2021

Attachment Properties

Use the Attachment properties to edit attachments and configure whether or not the attachments are displayed when the alarm is triggered.

 
action_zoom_plus_stroke Attachment properties
Figura: Attachment properties

Tabla: Attachment Properties

Component

Description

Display on alarm

Select True to to automatically open and display the attachment when the alarm is going from Normal to Alarm state.

Object reference

Enter the path to the item you want to attach to the alarm.

  • Archivos adjuntos de alarma
  • Adding an Attachment to an Alarm
  • Adding an Attachment to Multiple Alarms
  • Removing an Attachment from an Alarm
  • Removing Attachments from Multiple Alarms