earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: ​License Administrator, ​License Server
功能: 许可证管理
产品版本: 2.0, 2.1, 3.0, 3.1
2018/5/18

Backing Up Licenses

You back up licenses to easily restore them if something unexpected happens.

显示更多
action_close

Schneider Electric recommends backing up the License Server files on a regular basis. To back up the license files, copy all files in the folder to an external resource. This backup is primarily intended for cases when hardware or the operating system malfunctions.

Backed up licenses can only be restored on the same License Server that the files were backed up from. If you plan to move the licenses to another License Servers, you first have to return the licenses to the License Activtation Server and then activate them on the new License Server.

The License Server files are located in: \ProgramData\FLEXnet in Windows.

Licenses restored from a backup can be considered damaged by the License Server. 有关更多信息,请参阅 License Repair .

To back up licenses
  1. Close all EcoStruxure Building Operation applications, such as License Administrator, WorkStation, and Enterprise Server.

  2. On the License Server, browse to the folder \ProgramData\FLEXnet.

  3. Copy all files in the FLEX-net folder that start with taclic_ and paste the files onto your external backup resource.

  • Restoring Licenses
  • License Backup
  • Lost License
  • EcoStruxure Building Operation Software Requirements