earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: ​License Administrator, ​License Server
功能: 许可证管理
产品版本: 2.0, 2.1, 3.0, 3.1
2018/5/18

Restoring Licenses

You restore the license data from a backup to restore a corrupt or non-functioning License Server.

显示更多
action_close

Schneider Electric recommends backing up the License Server files on a regular basis. To back up the license files, copy all files in the folder to an external resource. This backup is primarily intended for cases when hardware or the operating system malfunctions.

Backed up licenses can only be restored on the same License Server that the files were backed up from. If you plan to move the licenses to another License Servers, you first have to return the licenses to the License Activtation Server and then activate them on the new License Server.

The License Server files are located in: \ProgramData\FLEXnet in Windows.

Licenses restored from a backup can be considered damaged by the License Server. 有关更多信息,请参阅 License Repair .

To restore licenses
  1. Close all EcoStruxure Building Operation applications, such as License Administrator, WorkStation, and Enterprise Server.

  2. ​On the License Server, browse to the the folder \ProgramData\FLEXnet\

  3. Paste all your backed up files to the FLEX-net folder.

    注释:
    • You may need to repair restored licenses before you check out the restored licenses. 有关更多信息,请参阅 Repairing a Network License .

You now restart the License Server so you can check out the restored licenses. 有关更多信息,请参阅 Restarting the License Server .

  • Backing Up Licenses
  • Repairing a Network License
  • Restarting the License Server
  • License Backup
  • Problem with the Licenses on the License Server
  • EcoStruxure Building Operation Software Requirements