Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.3, 2022
2021-07-23

Backup and Restore Manager on the Enterprise Server

Use the Backup and Restore Manager to supervise the backup settings in the EcoStruxure Building Operation software. You can also open this view in any EcoStruxure BMS server to view current and past backup information.

 
action_zoom_plus_stroke Backup and Restore Manager on the Enterprise Server
Rysunek: Backup and Restore Manager on the Enterprise Server

Tabela: Backup and Restore Manager

Component

Description

Status 

Displays the current backup status, such as backing up.

Last backup 

Displays the date and time of the last successful backup.

Backup sets path 

Displays the path to where the Enterprise Server stores all EcoStruxure BMS server backups.

Enable Automation Server purge 

Select to enable the Enterprise Server to purge the oldest backup of the automation server automatically when a new backup for that automation server is stored.

Number of Automation Server backup sets to store 

Enter the maximum number of backups that the Enterprise Server can store for each automation server.

Enable purge of local backup sets 

Select to enable the Enterprise Server to purge the oldest backup automatically when a new backup is stored.

Number of local backup sets to store 

Enter the maximum number of backups that the system can store for the Enterprise Server.

  • Automatic Purge of Backup Sets
  • Backup Options Dialog Box
  • Backup Set Properties – Basic Tab