earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 1.9
4/25/2017

Backup Sets

Backup sets are compressed backup files used for restoring data. Building Operation stores the local backup set for an Enterprise Server or SmartStruxure server devices in the Local folder within the Backup sets folder.

Backup Sets Location

Backup sets are stored in different locations for stand-alone systems and multi-server systems.

For more information, see Location of Backup Sets .

Backup Sets and Server Name

Building Operation associates each backup set with a particular SmartStruxure server name. Therefore, you should not rename a SmartStruxure server unless absolutely necessary. If you do rename a SmartStruxure server, the previous backup sets do not display in the Restore Options dialog box. You can view all the backup sets that are stored locally on an Enterprise Server. For more information, see Locating the Local Backup Path on the Enterprise Server .

Tip:

Going forward, you must create new backups for the renamed SmartStruxure server.

Backup Set Storage and Protection

SmartStruxure servers store backup sets in their local directories. By design, the average user may not easily locate these backup directories using a Windows-based file system. For convenience, you can save backup sets stored on SmartStruxure servers to WorkStation. After saving the backup set, you can also copy the file to another backup storage location.

For more information, see Backup Set Storage and Protection .

Backup Set Import from WorkStation

You import a backup set from WorkStation to replace a lost or incomplete backup set, or to add a backup set to a new SmartStruxure server.

For more information, see Backup Set Import from WorkStation .

Automatic Purge of Backup Sets

An Enterprise Server stores multiple local and remote backup sets. As a result, these sets can consume much needed space on the Enterprise Server. To resolve this problem, you can configure the Enterprise Server to remove outdated backup sets.

For more information, see Automatic Purge of Backup Sets .

  • Backup
  • Location of Backup Sets
  • Locating the Local Backup Path on the Enterprise Server
  • Automatic Purge of Backup Sets
  • Backup Set Storage and Protection
  • Backup Set Import from WorkStation
  • Diagnosing Backup or Restore Issues