earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Schedules
Product version: 2.0, 2.1, 3.0, 3.1
10/24/2018

Binding a Digital Value to a Digital Schedule

You bind a digital value to a digital schedule so the variable status follows the scheduled times.

Show More
action_close

A binding is a connection between two or more variables for data exchange. In its simplest form, a binding consists of a source and a destination. The destination reads the value from the source.

 
action_zoom_plus_stroke Binding diagram
Figure: Binding diagram

In EcoStruxure BMS, you typically bind source values to destination properties in objects such as programs, alarms, trend logs, and graphics. These objects frequently need to use values that exist somewhere else in the system.

Binding Examples

Bindings are used in schedules the same way that bindings are used throughout the system. You bind a schedule to a point in order to control the value with the schedule. The following examples demonstrate the different uses of schedules and bindings.

Analog Schedule

You bind an analog schedule to an analog output, such as a thermostat setpoint. When the schedule dictates a change in temperature, the system sends the output information to the setpoint for the thermostat to act on. For more information, see Binding an Analog Value to an Analog Schedule .

Digital Schedule

You bind a digital schedule to a digital output, such as a light switch. The system will switch the light on or off depending on the value set in the schedule. For more information, see Binding a Digital Value to a Digital Schedule .

Multistate Schedule

You bind a multistate schedule to a multistate output, such as an air handler. When the schedule dictates a change in air flow, the system will send the output information to the air handler depending on the value of the state set in the schedule. For more information, see Binding a Multistate Value to a Multistate Schedule .

To bind a digital value to a digital schedule
  1. In WorkStation, in the System Tree pane, select the variable or value that contains the digital value.

  2. On the Actions menu, click Edit bindings .

  3. In the Bindings View, in the Browser pane, select the folder that contains the digital schedule.

  4. Select the digital schedule that you want to bind to the digital value.

  5. Drag the digital schedule to the Binding column for the digital value.

     
    action_zoom_plus_stroke
  6. On the File menu, click Save .

  • Schedule Bindings
  • Bindings View