功能: 时间表
产品版本: 1.8
2016/10/13

Binding an Analog Value to an Analog Schedule

You bind an analog value to an analog schedule so the variable status follows the scheduled times.

显示更多
action_close

A binding is a connection between two or more variables for data exchange. In its simplest form, a binding consists of a source and a destination. The destination reads the value from the source.

 
action_zoom_plus_stroke Binding diagram
图: Binding diagram

In Building Operation, you typically bind source values to destination properties in objects such as programs, alarms, trend logs, and graphics. These objects frequently need to use values that exist somewhere else in the system.

Binding Examples

Bindings are used in schedules the same way that bindings are used throughout the system. You bind a schedule to a point in order to control the value with the schedule. The following examples demonstrate the different uses of schedules and bindings.

Analog Schedule

You bind an analog schedule to an analog output, such as a thermostat setpoint. When the schedule dictates a change in temperature, the system sends the output information to the setpoint for the thermostat to act on. 有关更多信息,请参阅 Binding an Analog Value to an Analog Schedule .

Digital Schedule

You bind a digital schedule to a digital output, such as a light switch. The system will switch the light on or off depending on the value set in the schedule. 有关更多信息,请参阅 Binding a Digital Value to a Digital Schedule .

Multistate Schedule

You bind a multistate schedule to a multistate output, such as an air handler. When the schedule dictates a change in air flow, the system will send the output information to the air handler depending on the value of the state set in the schedule. 有关更多信息,请参阅 Binding a Multistate Value to a Multistate Schedule .

To bind an analog value to an analog schedule
  1. In WorkStation, in the System Tree pane, select the program or folder that contains the analog value.

  2. On the Actions menu, click Edit bindings .

  3. In the Browser pane, select the folder that contains the analog schedule.

     
    action_zoom_plus_stroke
  4. Select the analog schedule that you want to bind to the analog value.

  5. Drag the analog schedule to the Binding column for the analog value.

  6. On the main toolbar, click the Save button

     
    action_zoom_plus_stroke
    .

  • Schedule Bindings
  • Analog Schedules