Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
Use the Alarm Trigger page to configure the trigger settings of the change of state alarm.
|
Component |
Description |
|
True |
Select to trigger the alarm when the monitored variable is equal to true. |
|
False |
Select to trigger the alarm when the monitored variable is equal to false. |
|
Monitored variable |
Enter the path to the variable that is monitored by the alarm. |
|
Disable alarm |
Select to disable the alarm, for example, before deployment. |
|
Alarm delay |
Enter the time, in seconds, the alarm has to be within the reset criteria before the alarm state is changed from alarm to reset. |
|
Reset delay |
Enter the time, in seconds, the alarm has to be within the alarm criteria before the alarm is triggered. |
|
Shunt variable 1 |
Enter the shunt variable that is used to enable or disable the alarm. Pour plus d'informations, voir Shunt Variables . |
|
Invert |
Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. Pour plus d'informations, voir Shunt Variables . |
|
Operator |
Select AND or OR to add logic between the first and the second shunt variable. Pour plus d'informations, voir Shunt Variables . |
|
Shunt variable 2 |
Enter the second shunt variable that is used to enable or disable the alarm. Pour plus d'informations, voir Shunt Variables . |
|
Invert |
Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. Pour plus d'informations, voir Shunt Variables . |