earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Fonctionnalités : Tendances
Version produit : 2.0, 2.1, 3.0, 3.1
25/10/2018

Configuring a Manual Trend Log

​You configure the properties of a manual trend log to meet the unique needs of your site.

Afficher plus
action_close

​The manual trend log records data that you manually enter. The manual trend log does not log a variable. Use this type of trend log when values from offline devices have to be manually registered to the trend log. For example, if you want to create a trend log that monitors an electricity meter that cannot be connected to the EcoStruxure BMS.

The default size of a manual trend log is 100 records.

 
action_zoom_plus_stroke Manual trend log schematic.
Figure : Manual trend log schematic.
Manual trend log meter functionality

A manual trend log can be created with initial meter settings. The manual trend log supports the meter change command and meter consumption calculation. You can view the last meter change information on the manual trend log object. Pour plus d'informations, voir Fonction de compteur .

To configure a manual trend log
  1. In WorkStation, in the System Tree pane, select the manual trend log you want to configure.

  2. On the File menu, click Properties .

  3. In the properties dialog box, click the Basic tab.

  4. Edit the basic properties:

    Table : ​Manual Trend Log Properties - Basic Tab

    Component

    Description

    Unit

    Enter the unit the trend log stores the records in.

     
    action_zoom_plus_stroke

    Click to open the configuration dialog box where you configure the property.

    Pour plus d'informations, voir Configure Dialog Box – Configuration Tab .

  5. Click the Meter Info tab.

  6. Edit the meter properties:

    Table : Meter Info Tab

    Property

    Description

    Is meter log

    Select True if the trend log meter function is active.

    Pour plus d'informations, voir Fonction de compteur .

    Meter change time

    Enter the time when the meter was changed.

    Meter change user

    Enter the name of the user account that changed the meter.

    End time

    Enter the time when the old meter was replaced.

    End value

    Enter the value the old meter had when it was replaced.

    Start time

    Enter the time when the new meter was installed.

    Start value

    Enter the value of the new meter when it was installed.

    Meter constant

    Enter the constant of the new meter. If the meter counts in kilo (10 3 ), the constant is 1000.

    Min value

    Enter the first value of the new meter after roll-over.

    Max value

    Enter the last value of the new meter before roll-over.

  7. Click OK .

  • Manual Trend Logs
  • Manual Trend Log Properties – Basic Tab
  • Configure Dialog Box – Configuration Tab
  • Adding a Trend Log Record to a Manual Trend Log
  • Fonction de compteur
  • Trend Log Does Not Start Record Due to the Start Condition