earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-C, AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Server, Project Configuration Tool
功能: 趋势
产品版本: 1.8
2016/10/13

Configuring a Manual Trend Log

​You configure the properties of a manual trend log to meet the unique needs of your site.

显示更多
action_close

​The manual trend log records data that you manually enter. The manual trend log does not log a variable. Use this type of trend log when values from offline devices have to be manually registered to the trend log. For example, if you want to create a trend log that monitors an electricity meter that cannot be connected to Building Operation.

 
action_zoom_plus_stroke Manual trend log schematic.
图: Manual trend log schematic.

To configure a manual trend log
  1. In WorkStation, in the System Tree pane, click the manual trend log you want to configure.

     
    action_zoom_plus_stroke
  2. Edit the properties:

    表格: ​Manual Trend Log Properties

    Component

    Description

    Unit

    Enter the unit the trend log stores the records in.

     
    action_zoom_plus_stroke

    Click to open the configuration dialog box where you configure the property. 有关更多信息,请参阅 Configure Dialog Box – Configuration Tab .

  3. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Manual Trend Logs
  • Manual Trend Log Properties
  • Configure Dialog Box – Configuration Tab
  • Adding a Trend Log Record to a Manual Trend Log
  • Trend Log Does Not Start Record Due to the Start Condition