You configure the properties of an interval trend log to meet the unique needs of your site.
In WorkStation, in the System Tree pane, click the interval trend log you want to configure.
Edit the properties:
Property |
Description |
Status |
Displays the status of the trend log. |
Enabled |
Displays True if the trend log is enabled. |
Logged variable |
Enter the variable you want to log. |
Delta |
Select the minimum value change that triggers a new record. For more information, see Interval Trend Log Delta . |
Activation variable |
Enter the variable that makes the trend log start recording values when the variable is True . For more information, see Trend Log Activation . |
Activation time |
Specify the time when the trend log is to start recording values. For more information, see Trend Log Activation . |
Interval |
Type how often to log the variable. The interval defines the time between two log records. |
Log size |
Select the number of records to store before old records are overwritten, including internal records generated by the trend log. For more information, see Log Record Storage . |
Clear when enabled |
Select True to clear the trend log when it is enabled. |
Click the Save button