Produits : License Administrator, License Server
Fonctionnalités : Gestion des licences
Version produit : 2024, 7.0
03/12/2024

Configuring the License Server Recovery Settings  

You configure License Server recovery settings to ensure that the License Server restarts if it unexpectedly stops. 

Afficher plus
action_close

License Server manages the administration of EcoStruxure Building Operation software licenses.

An EcoStruxure BMS running with EcoStruxure Building Operation Software licenses must contain at least one License Server. Use one License Server on every computer that runs a feature that require an EcoStruxure Building Operation software license.

License Server is a Microsoft Windows service named Building Operation License Server.

Configure the License Server to automatically restart if it unexpectedly stops. Pour plus d'informations, voir Configuring the License Server Recovery Settings   .

You can access License Server through a web interface. Pour plus d'informations, voir Accessing License Server Using the Interface .

With a default installation, the License Server port range is set to 27000-27009. A valid number is any unused port between 0 and 64000.

If the License Server uses other ports than the default port range 27000-27009, the port has to be added in front of the @ in the License Server address on the WorkStation, Enterprise Server, or Client tools.

To configure the license server recovery settings
  1. On the computer running License Server, open the Services management console.

    Déclaration

    In Windows, open the Run dialog box and type services.msc .

  2. Right-click Building Operation License Server .

  3. Select Properties .

  4. Click the Recovery tab.

  5. In the First failure box, select Restart the Service .

  6. In the Second failure box, select Restart the Service .

  7. In the Subsequent failures box, select Restart the Service .

  8. Click OK .

  • License Server