earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Como

Como


Produtos: License Administrator, License Server
Funcionalidades: Gestão de licenças
Versão do produto: 3.2, 3.3, 2022, 2023
15-07-2020

Configuring the Address to the License Server

You configure the address to License Server so Enterprise Server, WorkStation, or a client tool knows where to find available licenses to activate.

Nota

To configure the address to the License Server
  1. In License Administrator, click the Licenses server address view.

  2. In the License server address box, type @ and then type the address to the License Server.

    Nota
    • The address must begin with an @.

    • If you use a port other than the default port of 27000, type the port number in front of @. For example, 567@localhost.

    • Use a semicolon to separate addresses to different License Servers.

  3. Click Save .

Next time a WorkStation, client tool, or Enterprise Server starts, it activates available EcoStruxure Building Operation software licenses from the defined License Server.

Nota
  • The License Server address is configured individually on all WorkStations and Enterprise Servers.

  • Removing an EcoStruxure Building Operation Software Demo License
  • License Server Address View
  • Unable to Activate EcoStruxure Building Operation Software Licenses