earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: ​License Administrator, ​License Server
功能: 许可证管理
产品版本: 1.8, 1.9
2015/5/22

Configuring the Address to the License Server

You configure the address to the License Server so the Enterprise Server, WorkStation, or client tool knows where to find available licenses to check out.

注释:

显示更多
action_close

When you activate a license, the license is transferred from the License Activation Server to your License Server. When activating a license, details about the transaction and registration details are stored with the license on the License Server.

The examples in these sections are adaptable on all Building Operation systems including the systems where License Server, WorkStation, and Enterprise Server are located on the same computer.

The license activation procedure consists of four steps:

  • Request order information

  • Activate network license on License Server

  • Configure Enterprise Server’s address to the License Server

  • Configure WorkStation’s address to the License Server

Order Information Request

To receive order information from the License Activation Server, you need the Entitlement ID of the order. The entitlement ID is the designation that represents the license purchased by the customer. This ID is included in the Entitlement Certificate that is sent by e-mail when an order is approved.

有关更多信息,请参阅 Order Information Request .

Network Licenses Activation

To activate a network license means that a license is transferred from the License Activation Server, hosted by Schneider Electric, to your License Server. Once activated, the network license is available for use.

有关更多信息,请参阅 Network Licenses Activation .

Enterprise Server Address Configuration

After licenses are activated on the License Server, you configure the Enterprise Server connection to the License Server. The address to the License Server is defined either during the installation of Enterprise Server, through License Administrator, or Windows registry.

有关更多信息,请参阅 Enterprise Server Address Configuration .

WorkStation and Client Tools Address Configuration

After licenses are activated on the License Server you have to configure the Workstation and its client tools connection to the License Server, where licenses are available for check out. The address to the License Server is defined either during the installation of WorkStation, through License Administrator, or Windows registry.

有关更多信息,请参阅 ​WorkStation and Client Tools Address Configuration .

Network License Upgrade

When a new license version is released it is recommended that you upgrade your old versions. Customers that have signed up for the Building Operation Maintenance Subscription are automatically notified about the new upgrade and can directly activate the newest version. If your organization does not have the Building Operation Maintenance Subscription, contact your Building Operation vendor to place an upgrade order.

有关更多信息,请参阅 Network License Upgrade .

To configure the address to the License Server
  1. In License Administrator, click the Licenses server address view.

  2. In the License server address box, type @ and then type the address to the License Server.

     
    action_zoom_plus_stroke
    注释:
    • The address must begin with an @.

    • If you use a port other than the default port of 27000, type the port number in front of @. For example, 567@localhost.

    • Use a semicolon to separate addresses to different License Servers.

  3. Click Save .

Next time a WorkStation, client tool, or Enterprise Server starts, it checks out available network licenses from a defined License Server.

注释:
  • The License Server address is configured individually on all WorkStations and Enterprise Servers.

  • Removing a Local License or Returning a Network License
  • Network License Management
  • License Server Address View
  • Unable to Check Out License
  • ​License Server Address