earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: ​License Administrator, ​License Server
功能: 许可证管理
产品版本: 1.8, 1.9
2018/5/18

​License Server Address

​During the installation of License Administrator on WorkStations or Enterprise Servers, you need to type the network address to the License Server where network licenses are available for check out. The address to the License Server can later be entered or edited through License Administrator or directly in the Windows registry ​of the computer or Enterprise Server that hosts the licensed product.

In a 32-bit operating system, the License Server address is stored in the Windows registry key: HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\StruxureWare\License Administrator\TACLIC_LICENSE_FILE. In a 64-bit operating system, there is a separate area in the registry for all running 32-bit programs.

The address to a License Server must begin with @ and is either a hostname or IP address. If the communication to the License Server is through a port other than the default port range 27000-27009, the port number is defined in front of the @, Port-number@hostname.

表格: Example of License Server Address

Address

Description

19650@localhost

Connects to localhost through port 19650

@server2c.schneider-electric.com

Connects to License Server server2c.schneider-electric.com through a port in the default port range 27000-27009

14650@192.166.248.2

Connects to License Server 192.166.248.2 through port 14650

To separate License Server addresses in License Administrator, use a semicolon.

 
action_zoom_plus_stroke Example of License Server addresses in License Administrator
图: Example of License Server addresses in License Administrator

​In this example, @localhost refers to this computer, through port 19650. For example if a License Server and an Enterprise Server are located on the same computer, the network address of the Enterprise Server to the License Server is recommended to be @localhost.​

  • Licensing Overview
  • License Administrator
  • License System
  • Licenses
  • License Server Address View
  • Configuring the Address to the License Server