earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Como

Como


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmes
Versão do produto: 3.2, 3.3, 2022
15-10-2020

Configuring the Delay Time of an Alarm

You configure the time delay of an alarm ​to ​meet the unique needs of your site.

To configure the delay time of an alarm
  1. In WorkStation, in the System Tree pane, select the alarm object you want to configure.

  2. In the properties pane, click the Alarm Trigger tab.

  3. In the Alarm delay box, enter the time delay before an alarm is triggered.

  4. In the Reset delay box, enter the time delay before an alarm is reset.

  5. In the Changes have been made dialog box, click Yes to save the changes.

  • Time Delay
  • Create Variable Status Alarm Wizard – Alarm Trigger Page
  • Create Enumeration Alarm Wizard – Alarm Trigger Page
  • Create Matching Text String Alarm Wizard – Alarm Trigger Page
  • Create Sum Alarm Wizard – Alarm Trigger Page
  • Create Out of Reference Range Alarm Wizard – Alarm Trigger Page
  • Create Out of Range Alarm Wizard – Alarm Trigger Page
  • Create Multistate Alarm Wizard – Alarm Trigger Page
  • Create Change of State Alarm Wizard – Alarm Trigger Page