Configuring the Target of a Shortcut

Shortcuts created using the File-New submenu or the Context menu New command are not automatically configured with a target, therefore you must configure the target manually.

显示更多
action_close

When you have created a shortcut in a folder or on a SmartStruxure server using the File-New-Shortcut submenu or the context menu New-Shortcut option, you must then also assign a target to the shortcut. It is not necessary to assign a target to a shortcut after using any other shortcut creation method.

When you delete a target object, the forward reference in all shortcuts referencing that target object is removed. Also, the shortcut object icon changes to display the shortcut overlay icon only (a small arrow in a square).

When you delete a shortcut object, the (backwards) reference held in the target object is removed.

When you move a target object, the shortcuts referencing that target are updated with the new target path in their (forward) target object reference. When you move a shortcut object, the (backwards) reference held in the target object is updated with the new path.

When you rename a target object, the shortcuts referencing that target are updated with the new target path. If you rename a shortcut object, the (backwards) reference held in the target object is updated with the new path.

When you duplicate a shortcut object, the (backwards) reference held in the common target object is updated with the additional path to the new shortcut. 有关更多信息,请参阅 Configuring the Target of a Shortcut .

To configure the target of a shortcut
  1. In WorkStation, in the System Tree pane, right-click the shortcut object and select Shortcut Properties .

  2. Click the Basic tab.

  3. Edit the basic properties:

    表格: Basic Tab

    Component

    Description

    Target

    Enter the path of the target object (either directly, or by way of the browse button

     
    action_zoom_plus_stroke
    )

  4. In the Select Object dialog box, select a Path Type option (if required).

     
    action_zoom_plus_stroke

  5. Click Select .

  6. Click OK .

  • Shortcut Targets
  • Shortcut Properties – Basic Tab