earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Modalità

Modalità


Prodotti: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funzionalità: Tendenza
Versione del prodotto: 2023
21/05/2024

Configurazione del fuso orario in un grafico del Trend

Puoi visualizzare l'orario delle registrazioni nell'ora locale, nell'ora del server o nell'ora di un fuso orario predefinito. Modificando le impostazioni di fuso orario, faciliti l'interpretazione del timestamp.

Mostra di più
action_close

​In a trend chart, you can present the records of a trend log in different time zones: local time or a predefined time zone.

​A time zone is a region on the earth that has a uniform standard time, usually referred to as the local time. Local time is the UTC time plus the current time zone offset for the considered location. Some time zones also have an offset called DST added during the summer period. The DST offset is typically +1 hour.

Before you set the time zone for a trend chart, you should consider these settings:

  • Computer clock settings​

  • Regional settings

A computer clock displays time that has been set manually or by synchronizing to a time server. The computer clock time shows local time. Regional time displays the time of the selected location. Asynchronous computer clock time and regional time are not uncommon and can cause, for example, unexpected time discrepancies between time stamps on received values and the computer clock time.

​To adjust the automation server time, time zone, and DST, you have to access the automation server through a WorkStation.

Local Time

A trend chart presented in Local time displays trend logs with time stamps adjusted for the client computer time zone.

The client computer does not consider the local time of the EcoStruxure BMS server where the variable is logged. The same variable logged on EcoStruxure BMS servers in different time zones is displayed with matching time stamps for corresponding values.

 
action_zoom_plus_stroke Local time zone, schematic
Figura: Local time zone, schematic

Predefined Time Zone

A trend chart presented in a predefined time zone displays trend logs in the time of the selected time zone regardless of where the EcoStruxure BMS server is located.

The same variable logged on EcoStruxure BMS servers in different time zones are displayed with adjusted time stamps for corresponding values. Use predefined time zone when you need to compare trend logs on EcoStruxure BMS servers located in different time zones.​

 
action_zoom_plus_stroke Predefined time zone, schematic
Figura: Predefined time zone, schematic

Per configurare la modalità fuso orario in un grafico del Trend
  1. In WorkStation, nel riquadro Struttura di sistema , seleziona il grafico di trend da configurare.

  2. Nella visualizzazione del grafico di trend, sulla barra degli strumenti, fai clic sul pulsante Apri impostazioni del grafico trend

     
    action_zoom_plus_stroke
    .

  3. Nella finestra di dialogo Impostazioni del Trend chart , nel riquadro Fuso orario , seleziona un fuso orario per cui visualizzare i timestamp del grafico di Trend:

    • Seleziona Ora locale per visualizzare i timestamp in tempo reale dal punto di vista del cliente.

    • Seleziona un fuso orario predefinito per visualizzare i timestamp in tempo reale dal punto di vista del fuso orario selezionato.

  4. Fai clic su OK .

L'asse x è impostato in base al fuso orario selezionato.

  • Time Zone Modes in a Trend Chart
  • Icone eventi di un grafico del Trend
  • Trend Chart Settings Dialog Box – Axes Tab