You set the trend chart time span of the x-axis relative to the series current end point time to automatically adapt the trend chart to display the current time and the latest records within the specific time span.
In WorkStation, in the System Tree pane, select the trend chart you want to configure.
On the Trend Chart toolbar, click Open trend chart settings button
In the Time mode box, select Relative (to current time) .
In the Time span box, type the length of the x-axis to display before the current time .
Click OK .
The x-axis is now configured with a relative time span.